Technical FAQs

Ask a Question

Will the Altivar ATV58 show a fault without a keypad?

Yes, there is a red fault LED indicator on the front of the drive.
Also, the R1A and R1C contacts will open and the R1B & R1C contacts will close on fault condition or complete loss of power.
It is not possible to know the fault code without a keypad, serial communications or Powersuite software.

CTA-ID : 6801
Was this helpful?
What can we do to improve the information ?