Technical FAQs

Ask a Question

What main breakers are provided in a SU3040D300CB and SU3040D400FB 400A CSED All-In-One?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarification

Resolution:
These 400A CSED All-In-One panels are provided with one QDL22200 factory installed.  The factory installed QDL22200 feeds the 30 space/40 circuit loadcenter interior. Additional space is provided for the field installation of a second QDL main breaker, 100A maximum.


CTA-ID : 2027168
Was this helpful?
What can we do to improve the information ?