Technical FAQs

Ask a Question

What main breakers are provided in a SU3040D400CB, SU3040D400CN, SU3040D400FN, SU3040D400FB, RU3040D400CL, RU3040D400FL, RU3040D400CK and RU3040D400FK 400A CSED All-In-One panel?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarification

Resolution:
These 400A CSED All-In-One panels are provided with one QDL22200 factory installed. The factory installed QDL22200 feeds the 30 space/40 circuit loadcenter interior. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum.


CTA-ID : 2027165
Was this helpful?
What can we do to improve the information ?