Technical FAQs

Ask a Question

Can Powersuite connect to Altivar 58 drives through a Modbus network?

Yes. Powersuite allows connection to drives through Modbus networks.
The communication settings in Powersuite must match those on the drive.
Powersuite will only communicate with one drive at a time based on the Modbus address.
The PC must have an adapter to allow connection to the 2 wire RS485 Modbus network.

CTA-ID : 6795
Was this helpful?
What can we do to improve the information ?