Technical FAQs

Ask a Question

Can the Altivar 58 drives communicate with Magelis terminals?

Yes. Magelis terminals can typically be set up as Modbus masters. The Altivar 58 drives can communicate Modbus through the keypad port or by the Modbus card (VW3A58303U).
Magelis terminals can be programmed to exchange data with the registers in the drive in a similar way as a PLC.


CTA-ID : 6793
Was this helpful?
What can we do to improve the information ?