Technical FAQs

Ask a Question

Can the Altivar ATV58 keypad be mounted in a wet environment?

No. The VW3A58101U keypads are rated for IP 20 which is similar to NEMA 1. They should be protected from moisture, direct sunlight and dust.
The remote mount kit VW3A58103 is rated for IP 65. This is similar to NEMA 12 or 3R. However, it is not advisable to use it in outdoor applications due to damage from sunlight and temperature extremes.

CTA-ID : 6787
Was this helpful?
What can we do to improve the information ?