Technical FAQs

Ask a Question

What tenant circuit breakers can be used in type EZMR or EZMH ringless type 1-Phase OUT, 225A maximum branch units?

2-Pole only type QBP-TM (70A ? 225A), QDP-TM (70 ? 225A), QGP-TM (70A ? 225A) and QJP-TM (70 ? 225A) bolt-in circuit breakers.
2-Pole only type QO (40 ? 125A), QO-VH (40 ? 125A) and QOH (40A ? 125A) plug-in circuit breakers that require the use of a plug-in to bolt-on adapter kits part number EZM125QOA (order separately).



CTA-ID : 2026886
Was this helpful?
What can we do to improve the information ?