Technical FAQs

Ask a Question

What should the temperature range be on the QED switchboards in use ?

The temperature range per UL891 is 40 to 105 degrees C



 
Was this helpful?
What can we do to improve the information ?