Technical FAQs

Ask a Question

Do the Altivar 58 Type H, Type F or FLEX58 drives include the keypad display?

No. The keypad must be ordered separately. The keypad part number is VW3A58101U.
Keypads are included with Econoflex, Type N, Type FVC and 58M drives unless otherwise specified.


CTA-ID : 6746
Was this helpful?
What can we do to improve the information ?