Technical FAQs

Ask a Question

Do the electronic boards in the Altivar ATV58 unit have conformal coating on them?

The electronic boards in the Altivar 58 drives are rated according to pollution degree specifications below.
They have conformal coating in areas of the board where it is needed to comply with these standards.

ATV58HU09M2?D12M2 and ATV58HU18N4?D23N4: Pollution degree 2 conforming to IEC 60664-1, EN50718, and NEMA ICS-1.

ATV58HD16M2?D46M2 and ATV58HD28N4?D79N4: Pollution degree 3 conforming to IEC 60664-1, EN50718, and NEMA ICS-1.

ATV58HC10N4X?C33N4X: Pollution degree 2 conforming to IEC 60664-1, EN 50718, and NEMA ICS-1.

Please protect the drive controller against dust, corrosive gas, and falling liquid.


CTA-ID : 6454
Was this helpful?
What can we do to improve the information ?