Technical FAQs

Ask a Question

What is the projection of the HVL switch operating handle in the closed (up) position?

The handle for the Over Toggle Mechanism (OTM) projects out 4.0`` in the closed position.
The handle for the Stored Energy Mechanism (SEM) projects out 5.0`` in the closed position.

CTA-ID : 2026867
Was this helpful?
What can we do to improve the information ?