Technical FAQs

Ask a Question

Are the NSJ and Powerpact D frame UVR devices ``kiss-free?``

The Compact NSJ and Powerpact D frame do have kiss-free UVR devices. This means if the UVR has no power, operation of circuit breaker closing mechanism will not permit the main contacts to touch, even momentarily.


CTA-ID : 2026865
Was this helpful?
What can we do to improve the information ?