Technical FAQs

Ask a Question

Is HC4286WP the correct weatherproof enclosure for use with HCM3691-6MP?

Issue:
Is HC4286WP the correct weatherproof enclosure for use with HCM3691-6MP?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product selection.

Resolution:
No you need to use the HCP3686-6M interior and HC4286WP because we don`t offer an Nema 3R enclosure for use with the HCM36916MP interior.


CTA-ID : 2026731
Was this helpful?
What can we do to improve the information ?