Technical FAQs

Ask a Question

Want to connect single phase input power to the ATV66 drive to do programming only before the three phase power is available to be applied, why does Altivar ATV66 lose parameter settings every time power is cycled?

Apply line power only to CL1 and CL2 to save parameter settings.

CTA-ID : 7066
Was this helpful?
What can we do to improve the information ?