Technical FAQs

Ask a Question

Does Square D offer an additional internal barrier for 30A and 60A (240V), Series F safety switches?<br />

Yes, please see publication number 40281-353-02 for details. This is located in the technical library under publications.

CTA-ID : 2026420
Was this helpful?
What can we do to improve the information ?