Technical FAQs

Ask a Question

Are there any auxiliary contacts standard on the Altistart ATS46 or ATS48 unit?

There are relay contacts built into the soft starter.  These can be used to indicate running status or other conditions as programmed.
If additional contacts are needed relays can be added to the control circuit. Contact your local Square D field office. Additional relay contacts can be added to enclosed soft starter packages.


CTA-ID : 7379
Was this helpful?
What can we do to improve the information ?