Technical FAQs

Ask a Question

What special features are provided with the 1635 circuit breaker suffix?

This suffix encompasses three features: 50 degree ambient temperature calibration, auxiliary contacts (2-NO, 2-NC) and 120 Vac undervoltage trip.


CTA-ID : 2026068
Was this helpful?
What can we do to improve the information ?