Technical FAQs

Ask a Question

What is the difference between the 9001SKY6 and 9001SKY600 control station?

9001SKY6 is six hole 30mm polymeric control station.  The 9001SKY600 is same control station with assembled operators by Square D.  9001SKY600 is not a part number you can order.  Customer must furnish a 9001 Control Station Key Sheet with order.  Key sheet can be obtained from Customer Service or local field office. Also can be found in the Push button catalog 9001CT0001.


CTA-ID : 2026580
Was this helpful?
What can we do to improve the information ?