Technical FAQs

Ask a Question

Can the ALAMP ammeter/trip indicator store various fault information from multiple trips of the PXF or PEF breaker ?

No, this module only retains the trip current level from the last overload, short circuit or ground fault occurrence. Once the on-board reset button is pressed that data is lost .

CTA-ID : 2026417
Was this helpful?
What can we do to improve the information ?