Technical FAQs

Ask a Question

Where can one find a list of triple-rated 9070 Type T and TF Industrial Control Transformers?

Issue:
9070 type T and TF style Industrial Control Transformers can have triple rated primaries and secondaries

Product Line:
LV Transformers

Environment:
Applies to Industial Control Transformers by SquareD/Schneider Electric

Cause:
 Industrial Control Transformers can have primary and secondary windings rated for several voltage levels

Resolution:

The triple rated voltage codes are D1, D5, D12, D24, D31, D32, D50, D65, and D95.  Several of the triple ratings are printed in the current Digest 177


CTA-ID : 2026415

Was this helpful?
What can we do to improve the information ?