Technical FAQs

Ask a Question

What is the UL file number for QOCGK2, QOCRBGK1 and QORBGK2 ?

Issue:
Codes & Standards

Product Line:
Load Center Accessory

Cause:
UL Standards

Resolution:
The Square D Generator Circuit Breaker Interlock Kit, catalog number QOCGK2, QOCRBGK1 and QORBGK2 is a UL Recognized Component listed in UL File E6294, Vol. 7, Section 16, when installed in a listed QO Load Center (UL file E6294, Vol. 8). The QOCGK2, QOCRBGK1 and QORBGK2 do not carry their own UL mark.


CTA-ID : 2026201
Was this helpful?
What can we do to improve the information ?