Technical FAQs

Ask a Question

What is the coil consumption or burden for the Tesys LC1D40__ through LC1D95__ contactors or LC2D40__ through LC2D95__ reversing contactors with AC Coils?

Product Line:
 
Tesys D line Contactors
 
Resolution:
 
For 50/60 hertz coils - Inrush = 245 VA and Sealed = 26 VA.
For 60 hertz coils - Inrush = 220 VA and Sealed = 22 VA.
For 50 hertz coils - Inrush = 200 VA and Sealed = 20 VA.


 
Was this helpful?
What can we do to improve the information ?