Technical FAQs

Ask a Question

Are the EZM and MP meter stacks Nema 3R?

Yes, the current design EZM and MP devices are NEMA 3R. The exception to this is the bussed corner section for EZM, and the busway tap EZM main devices.

CTA-ID : 2026571
Was this helpful?
What can we do to improve the information ?