Technical FAQs

Ask a Question

What is the part number for a 4 inch adjustable lenght arm with 2 inch roller for an XCKJ limit switch ?

Use a ZCKY49. This device has a distance of 3.91 inches from the center of the hub to the outside of the wheel which is 50 mm in diameter.


CTA-ID : 2026182
Was this helpful?
What can we do to improve the information ?