Technical FAQs

Ask a Question

Has the HVL/cc switch been tested for 1000V at 400Hz?

Yes, the HVL/cc switch was tested in France and is rated at 3300V 200A at 400Hz.


CTA-ID : 2026195
Was this helpful?
What can we do to improve the information ?