Technical FAQs

Ask a Question

What is the height of the operating handle for HVL/cc switchgear?

5/15kV Indoor Application A - Handle Height - 51.75`` Add 4`` for Outdoor
5/15kV Indoor Application B - Handle Height - 38.37`` Add 4`` for Outdoor
25/38kV Indoor Application A - Handle Height - 64.74`` Add 4`` for Outdoor
25/38kV Indoor Application B - Handle Height - 51.43`` Add 4`` for Outdoor
Note for Outdoor units, the operator will stand on the floor above the base channel to operate the switch.


CTA-ID : 2026046
Was this helpful?
What can we do to improve the information ?