Technical FAQs

Ask a Question

What is the recommended rod and float kit for a 9036DW31 ?

Use a 9049A6 (stainless float /brass rod and stops ) kit , A6A ( stainless float / aluminum rod / brass stops ) kit or A6S (stainless float & rod & stops) kit . These kits all have 7`` diameter floats tapped at the top . Alternate kits with 7``diameter center hole floats would be the 9049A6C, A6CA and A6CS . Add 9049T1 or T1S or T1A 2 1/2 foot extensions to go beyond 5 feet.

CTA-ID : 2026037
Was this helpful?
What can we do to improve the information ?