Technical FAQs

Ask a Question

Can you replace the clamp for the shaft on a 9007C54B2S9? Customer uses 3/16`` diameter rod.

Yes, 9007R16 is the `clamp` which holds customer-supplied 3/16`` rod of appropriate length. In addition, the S9 hub is available separately as 9007S9.

CTA-ID : 2026565
Was this helpful?
What can we do to improve the information ?