Technical FAQs

Ask a Question

Can an outdoor NEMA 3R rated Air Conditioner Disconnect be used indoors?

Yes, an outdoor NEMA 3R device can be used in an indoor, NEMA 1 General Purpose application.


CTA-ID : 2026394
Was this helpful?
What can we do to improve the information ?