Technical FAQs

Ask a Question

What is the peak surge current rating of a SDSB1175C?

The maximum single impulse current withstand rating is 60KA per phase.


CTA-ID : 2026389
Was this helpful?
What can we do to improve the information ?