Technical FAQs

Ask a Question

What type of overload relay is supplied with the Class 8536 Type vacuum starter?

Available exclusively with Class 9065 Motor Logic Feature Base solid state overload relays.


CTA-ID : 2026384
Was this helpful?
What can we do to improve the information ?