Technical FAQs

Ask a Question

What is the catalog number for a NEMA 4, 4X, 5, 3, 3R enclosure for the H and J Frame breakers?

Issue:  
What dusttight enclosures are available for the Powerpact H and J frame circuit breakers?  

Product line: 
Molded case circuit breakers

Environment:  
Powerpact H and J frame circuit breaker enclosures

Resolution:  
The catalog number is a J250DS for a NEMA 4, 4X, 5 Type 304 Stainless Steel enclosure or a J250SS for a NEMA 4, 4X, 5 Type 316 Stainless Steel enclosure.
Note that these are only available in surface mount.  
Was this helpful?
What can we do to improve the information ?