Technical FAQs

Ask a Question

On an EZML112225 branch unit where is the 5th Jaw located?

The 5th Jaw in an EZML112225 is located at the 9:00 o`clock position, and is movable to the 3:00 or 6:00 o`clock position with one mounting screw.




CTA-ID : 2026186
Was this helpful?
What can we do to improve the information ?