Technical FAQs

Ask a Question

Are the Class 8910 Type DP__ & Type DPA__definite purpose controller control coils continuous duty rated?

Issue:
Are the Class 8910 Type DP__ & Type DPA__definite purpose controller control coils continuous duty rated?

Product Line:
Definite purpose contactors

Environment:
Products sold and used in the United States

Cause:
Continuous voltage being put across the coil

Resolution:
Yes.


CTA-ID : 992
Was this helpful?
What can we do to improve the information ?