Technical FAQs

Ask a Question

Customer wants to know if a breaker will still trip if the breaker is locked into the on position?

Yes. The circuit breaker standard UL489 requires breakers to be ``trip - free,`` meaning they can still trip if the handle is held in the ON position.

CTA-ID : 2026376
Was this helpful?
What can we do to improve the information ?