Technical FAQs

Ask a Question

Can the Multi 9 C60N UL489 breakers be used with the 14803 busbar?

No, because the UL 489 Breakers are taller, it prevents the busbar from reaching down far enough for connection, therefore they cannot use the 14803 busbar with these breakers.


CTA-ID : 2026370
Was this helpful?
What can we do to improve the information ?