Technical FAQs

Ask a Question

DUPLICATE SEE FA162178 - What is the catalog number for the NEMA 12/3R, 5 enclosure for the H and J frame breakers?

THIS IS A DUPLICATE SEE FA162178

Issue:

Product design features

Product Line:
Circuit Breaker Enclosures

Environment:
Enclosure selection

Cause:
Application

Resolution:

The catalog number is a J250AWK.


CTA-ID : 2026365
Was this helpful?
What can we do to improve the information ?