Technical FAQs

Ask a Question

Is the HCR-U interior an I-Line panel?

Issue:
Is the HCR-U interior an I-Line panel?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, this is a new I-line panelboard that superseded the HCWM-U. See Digest 173 page 8-23.


CTA-ID : 2026020
Was this helpful?
What can we do to improve the information ?