Technical FAQs

Ask a Question

Does CU12L400CB include incoming lugs?

No, it has studs to mount separately supplied lugs on 1/2`` studs with NEMA 1 - 3/4`` spacing. Consider using our catalog number CMELK4 , which includes four lugs, each of which accepts a single # 2 to 600MCM aluminum or copper cable.


CTA-ID : 2026018
Was this helpful?
What can we do to improve the information ?