Technical FAQs

Ask a Question

Can the XVBC9M (or XVBC9B) sounder be programmed with different tones like the XVPC09** ?

The XVB has just 2 tones (steady or intermittent ) and 4 volume levels between 75 and 90db . In contrast , the XVP has 10 tone levels and several volume levels .

CTA-ID : 2026148
Was this helpful?
What can we do to improve the information ?