Technical FAQs

Ask a Question

Are lugs available for a QO1816M200FTRB to accept 2 conductors per phase?

There are no optional lugs for this loadcenter. The standard lugs will accept (1) #4 AWG - 250 KCMIL conductor per phase and neutral.


CTA-ID : 2026135
Was this helpful?
What can we do to improve the information ?