Technical FAQs

Ask a Question

Can MPL32225 be fed from the top?

Yes, it can be fed from either overhead or underground. The top endwall has provisions for (2) A-L type hubs which include a factory-provided ACPL closing plate. A-L type hubs need to be ordered separately.


CTA-ID : 2026013
Was this helpful?
What can we do to improve the information ?