Technical FAQs

Ask a Question

What is the coil burden for the 8501KF and 8501KFD relays?

It is 3.6 VA inrush and 2.5 VA sealed for the AC coils and 1.5 watts standard, 3 watts maximum for the DC coils.

CTA-ID : 2026558
Was this helpful?
What can we do to improve the information ?