Technical FAQs

Ask a Question

Can you use a PQ3620G at 174 full load amps?

No. There is a label inside the PQ3620G. It says ``Continuous load current not to exceed 80% of the rating of fuses employed in other than motor circuits.``

CTA-ID : 2026556
Was this helpful?
What can we do to improve the information ?