Technical FAQs

Ask a Question

What is the difference between QO300 and QOU300?

Both are molded case switches, neither provide overload protection or short circuit protection.
QOU is a din-rail or unit-mounted type and the QO is a plug-on type.

CTA-ID : 2026541
Was this helpful?
What can we do to improve the information ?