Technical FAQs

Ask a Question

What are dimensions of the slip on connector (form U2) for the 9013FSG. It is a 1/4 inch male spade?

The slip-ons are indeed quarter inch male spade . Also 0.032 inch thick and made out of brass. They are the standard slip-on connector.

CTA-ID : 2026348
Was this helpful?
What can we do to improve the information ?