Technical FAQs

Ask a Question

What replacement parts are available for a PQ4220G plug-in unit?

Only the Load Base Assembly is available. It is p/n 45201-229-50. This assembly includes the plastic base, lugs and load side fuse clips for 1 phase. If customer wants to replace all 3 phases , 3 assemblies would need to be ordered. This replacement is for Series 5 plug-in units only.


CTA-ID : 2026337
Was this helpful?
What can we do to improve the information ?