Technical FAQs

Ask a Question

Does Square D make an adaptor for installing the new Powerpact Q-Frame breakers in older EZM Branch devices that used the old QE type breakers?

Issue:
Old Style design EZM metering

Product Line:
EZM Metering

Environment:
Tenant breakers

Cause:
replacement tenant breaker

Resolution:
Square D does NOT make any type of adaptor for using the new Powerpact Q-frame breakers in the old EZM branch devices that used the QE type tenant breakers. 

NOTE: DEPENDING on the existing EZM catalog numbers, the customer could potentially use a transition section(see digest 176 page 2-15) for attaching the OLD EZM to NEW EZM and then obtain a complete new current design EZM Branch device with the current design tenant breakers. Since we cannot know in reference to the grade level(or floor) where the old EZM is mounted, it is recommended the customer obtain the drawings for the transition section and new EZM branch device(s), BEFORE obtaining any equipment to ensure the new EZM can be mounted appropriately with the OLD, in reference to the grade level(or floor). Also, to make sure they obtain the appropriate new EZM  that is APPROVED by the local Utility company.


CTA-ID : 2026132
Was this helpful?
What can we do to improve the information ?