Technical FAQs

Ask a Question

What is the difference between the QU816D400CL and QU816D400SL?

Issue:
product comparison

Product Line:
Combination Service Entrance Device

Environment:
Device Mounting

Cause:
Product features

Resolution:

The only difference between the QU816D400CL and QU816D400SL, is the mounting of the device. The device with suffix "SL" is Surface Mount ONLY and the device with suffix "CL" is combination Surface OR Semi-flush Mount. BUT for the semi-flush mounting there is a flange kit required, part number FK400(order kit separately)


CTA-ID : 2025991
Was this helpful?
What can we do to improve the information ?