Technical FAQs

Ask a Question

Can the cover of a LA100S or LA400S enclosure be padlocked to prevent access to the interior?

The cover of these NEMA 1 enclosures is attached to the enclosure with cover mounting screws. The circuit breaker handle is accessible through an opening in the cover. The cover cannot be padlocked since it is not of a hinged design. For an application requiring a padlockable cover, consider a LA400R (NEMA 3R), LA400A (NEMA 12K), LA400AWK (NEMA 12) or LA400DS (NEMA 4/4X/5).

CTA-ID : 2026536
Was this helpful?
What can we do to improve the information ?